Add a Certificate to the Server Certificates List

You use the Connection Security section of the Geo SCADA Expert Server Configuration Tool to set up your server's certificate settings for communications with the other servers and clients on your system (see Configure the Connection Security Settings).

In order for the server to use a server certificate from a trusted certification authority, you have to load that certificate into the Windows certificate store on the server machine, and add that certificate to the server's Server Certificates list.

To add a certificate to the Server Certificates list:

  1. Access the Geo SCADA Expert Server Configuration Tool.
  2. Expand the System Configuration branch.
  3. Select the Connection Security option to access the Connection Security settings.
  4. Select the Add button below the Server Certificates field. (The button is only available for use when the Use Temporary Certificates check box is clear.)

    The Add Server Certificates window is displayed.

  5. Use the window to add the required certificates:
    1. Use the Certificate Store Location field to specify whether the server certificate has been loaded into the:
      • Current User certificate store.
      • Local Machine certificate store.
    2. Use the Certificate Store field to specify the actual store in which the certificate is loaded. This will typically be the 'My' store.
      Certificates that are loaded into the specified store are displayed in the Certificates field.
  6. Select the required certificate from the list, followed by the OK button.
    The Add Server Certificates window is closed and the selected certificate is added to the Server Certificates field in the Connection Security section of the Server Configuration Tool.
  7. Repeat the above procedure for any further server certificates that the server is to use.
  8. Apply the changes to the server.

  9. Perform the same procedure on any other servers in your system.

Understand the Certificates Field

The Certificates field on the Add Server Certificates window displays the following information about each certificate:

Understand the Server Certificates Field

The Server Certificates field in the Connection Security section of the Server Configuration Tool displays the following information about each certificate:


Disclaimer

Geo SCADA Expert 2021