Delete an Event

This section applies to Schedules other than Simple Schedules.

To delete an event from a Schedule:

  1. Display the Schedule in Design Mode.
  2. Either:
    1. Double-click on the event that you want to remove.
      The event indicator is removed from the Schedule Display.
    2. Repeat step (i) for any other events that are now obsolete.

    Or:

    1. Display the Schedule Times Window.
    2. Select the event that you want to remove.

    3. Select the Remove button.
      The entry is removed from the list in the Schedule Times window.
    4. Repeat steps ii to iii for any other events that are now obsolete.
    5. Select the OK button to remove the obsolete events from the Schedule Display.
  3. Save the configuration.

Disclaimer

Geo SCADA Expert 2021