Simple Schedule

On a Simple Schedule, you specify the action(s) that are to trigger on Schedule execution. Unlike other types of Schedule, you do not add events to a Simple Schedule—any actions associated with a Simple Schedule execute at the offset and frequency that you specify, using fields on the Schedule Form (see Define when a Simple Schedule Executes).

You need to configure a separate Simple Schedule for any action(s) that require triggering at different rates or offsets to other scheduled action(s).

Further Information

Set up a Schedule.


Disclaimer

Geo SCADA Expert 2021