Generate a Profile’s Data Programmatically

You can plot a Time Profile’s change in value by manually adding vectors to the Profile’s graph (see Edit a Time Profile), or you can:

Use the SetVectors method to modify a Profile’s vectors programmatically using a custom program, Logic, or script. The SetVectors method has these arguments:

To successfully modify a Profile’s vectors programmatically:

If any of the above are not adhered to, the method call will be unsuccessful and Geo SCADA Expert will not modify the Profile’s vectors.

For an example that demonstrates how a Time Profile’s vectors might be generated programmatically, see Use a VBScript Program to Modify a Time Profile’s Vectors Programmatically.

Further Information

Using Geo SCADA Expert Script.

Server Automation.


Disclaimer

Geo SCADA Expert 2021