Report Value

Associated with: Master Station Accumulators for which Geo SCADA Expert logs data on a Timed Report basis

This status attribute indicates the Accumulator total that Geo SCADA Expert last logged on a Timed Report basis. Timed Report logging is configured using the Accumulator Form’s Timed Report properties (see Specify the Frequency with which Geo SCADA Expert Stores Timed Report Values).

Use the attribute in conjunction with the Report Quality and Report Time status attributes.


Disclaimer

Geo SCADA Expert 2021