Using the Color Window to Define a Color

Each Geo SCADA Expert system is supplied with sets of default colors. These sets include:

You can use the default colors on your system or choose to replace any of the colors with custom colors. You can also use a custom color to indicate a particular Point or Forecast state, in place of the default ‘Normal’ state color (see Defining a Custom State Color).

If you decide to use a custom color, you will need to use the Color window to specify the color that you want to use. This section explains how to use the Color window (see Using the Color Window). For information on accessing the Color window, see the appropriate section listed above.

When you specify a custom color, ensure that the color that you choose is not identical to, or could be confused with, another color on the system.

Further Information

Define the Colors for Point Trends

Change the Marker Colors on Trends


Disclaimer

Geo SCADA Expert 2021