Optionally Associate one or More Profiles with the Point

Use the fields within the Profiles section of the Analog Point tab to specify whether any of the point’s limits and/or current value are profile-controlled. (A DNP3 SCADAPack Analog point’s current value can be profile-controlled providing that point has a Point Type other than ‘Physical Input’.)

Depending on the outstation’s Profile Type, DNP3 SCADAPack analog points can use either:

Fields that do not apply to the specified Profile Type are ‘grayed out’ and unavailable for use.

With either type of Profile, use the Historic check box to specify whether Geo SCADA Expert is to store profile values historically.

For more information, see Specify Whether any Profiles are Used to Change a Point’s Limits or Current Value.

Remember that various Limitations and Restrictions have to be taken into account in order to associate Profiles successfully with a DNP3 SCADAPack point.


Disclaimer

Geo SCADA Expert 2021