Associated with: Outstations, including Slave outstations
This status attribute indicates whether communications between the driver and the outstation is healthy.
Possible States: Displays one of the Standard Alarm States.
If this attribute displays an alarm condition, but the outstation’s Channel State Alarm attribute indicates a healthy channel, this suggests that Geo SCADA Expert has detected a problem with the outstation, rather than the channel.
Also see State.
For information on resolving communications problems, see Troubleshooting in the Geo SCADA ExpertGuide to Advanced Drivers.