Introduction to the EtherNet/IP Driver

This driver is an advanced driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring EtherNet/IP items and features in the Geo SCADA Expert database.

The guide also contains information for:

Document Scope

This guide explains the configuration, features and database items that are specific to Geo SCADA Expert’s EtherNet/IP driver. The EtherNet/IP driver enables Geo SCADA Expert to communicate with supported ranges of Allen-Bradley controllers using the EtherNet/IP protocol. (For information about the ranges of Allen-Bradley controllers that the driver supports, see Configure an EtherNet/IP Outstation.)

The EtherNet/IP driver documentation:

NOTE: There are no driver-specific pick actions for database items on this particular driver. However, users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions in the Geo SCADA Expert Guide to Core Configuration). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).


Disclaimer

Geo SCADA Expert 2021