OPC Historic Aggregates (Algorithms)

OPC historic aggregates are calculations that can be applied to sets of historic data. For example, you can use the 'Max' OPC historic aggregates to calculate the maximum value in a set of historic data.

To avoid confusion with database aggregates, we refer to the calculations that can be performed on historic data as historic algorithms. But in the OPC standard, these calculations are called OPC Historic Aggregates.

The table below lists the Algorithm options. You can access further information by clicking on the entry in the Algorithm column.

Take care when entering the names of algorithms manually. Use the table below to determine whether the algorithm names comprise single words, multiple words with spaces, or are camel case (also known as 'medial capitals').

Take care with End and End Last Historic Algorithms used on clients, or with Geo SCADA Expert features, that run in Local Time with Daylight Saving Time. Ensure that the start and end times specified for the sample interval do not coincide exactly with the time at which the clock jumps backward. Include a small offset in the sample time, to offset the calculation to avoid the sample end or start time exactly matching the time that the clock jumps backward at the transition from Daylight Saving Time to Standard Time. A small offset of 1s or even 1ms should suffice. For more information about Daylight Saving Time, see The Effects of Daylight Saving Time Adjustments.

Algorithm Option Algorithm Description

1 Hour Moving Average

1hAverage

The average value over an hour period that starts at the beginning of the sample.

24 Hour Moving Average

24hAverage

The average value over a 24 hour period that starts at the beginning of the sample.

8 Hour Moving Average

8hAverage

The average value over an 8 hour period that starts at the beginning of the sample.

Average including last interpolated value

Average Interpolated

The average of the values in the sample. The average includes the interpolated value at the start of the interval.

Average including last value

Average Last

The average of the values in the sample. The average includes the last value reported before the start of the interval.

Average of absolute differences between consecutive values

Moving Range

The sum of the absolute differences between each pair of values in the sample.

Average of values

Average

The average value of the values in sample (the sum of the values divided by the number of values).

Count of values

Count

The number of raw values in the sample.

Difference of first and last value

Delta

The last value minus the first value in the block of data. Produces a zero value if both values are the same; a negative value if the last value is smaller than the first; and a positive value if the last value is larger than the first.

Difference of maximum and minimum value

Range

The difference between the maximum value and the minimum value in the sample.

If only one value exists in the sample, a zero value is returned.

Duration in which data is bad

DurBad

The duration (in seconds) of bad data in the sample.

(Values for which the quality is Uncertain are not included.)

Duration in which data is good

DurGood

The duration (in seconds) of good data in the sample.

Interpolated value

Interpolated

This is a calculation to estimate a value that is not included in the sample.

Geo SCADA Expert uses straight line (linear) interpolation to calculate an interpolated value at the start of the specified interval.

Geo SCADA Expert estimates the interpolated value using the last known value before the start of the interval, and the first known value after the start of the interval.

Last value in the data for the interval

End Last

The last good quality value in the sample (sample).

Maximum including last interpolated value

Max Interpolated

The largest value in the sample (including the interpolated value at the start of the interval).

Maximum including last value

Max Last

The largest value in the sample (including the last known value before the start of the interval).

Maximum value

Max

The largest value within the sample.

Maximum value and time stamp

MaxTime

The largest value within the sample. The value is time stamped with the time at which it occurred. (The time is not displayed on Mimics or Data Grids, and so on.)

Minimum including last interpolated value

Min Interpolated

The smallest value within the sample, including the interpolated value at the start of the interval.

Minimum including last value

Min Last

The smallest value within the sample, including the last known value before the start of the interval.

Minimum value

Min

The smallest value within the sample.

Minimum value and time stamp

MinTime

The smallest value within the sample. The value is time stamped with the time at which it occurred. (The time is not displayed on Mimics or Data Grids, and so on.)

Moving Range MovingRange The sum of absolute differences between each pair of values within the sample.

Percent in which data is bad

PerBad

The percentage of the data interval during which the quality of data is Bad.

Percent in which data is good

PerGood

The percentage of the data interval during which the quality of data is Good.

(1 = 100%)

Standard deviation of values

StdDev

The 'spread' of the values about their mean value.

Stepped analog

Stepped

Returns the last value before the start of the specified interval. This aggregate is included for backwards compatibility with old-style Trends.

Sum of values

Sum

The sum of the historic values in the sample.

Time-weighted average

Time Average

An average value for the sample, taking into consideration the amount of time the data source remained in each value.

Totalized value (Time Integral)

Total

The totalized value of the data in the sample.

Value at end of the interval

End

The last value in the sample.

Value at start of the interval

Start

The first value in the sample.

Variance of values

Variance

The square of the standard deviation of the values.

For more information on how the algorithms are calculated, which values are included in a sample, and how time stamps are applied to processed historic values, see Built-In Historic Algorithms for Processed Historic Data in the Geo SCADA Expert Guide to Trends.

Example: Referencing an OPC Historic Tag in an Expression

The tag for calculating the average value of an analog point, AIP4 within the group 'SCADAPack Modbus Direct' (itself within the group 'SCADAPack Modbus Group'), over a 2-hour period, starting three hours ago is:

"SCADAPack Modbus Group.SCADAPack Modbus Direct.AIP4;Average;H-3H;2H"

You can enter this tag manually, by typing it into the Expression window, or you can use the Select Historic Tag window to locate the data source and specify the required parameters for the tag.

Geo SCADA Expert also supports any custom historic algorithms that have been created on your system (see Historic Algorithms (Custom) in the Geo SCADA Expert Guide to Server Administration). When you are configuring a Historic item, any custom historic algorithms are included in the list of available algorithms.


Disclaimer

Geo SCADA Expert 2021