Specify a Logical Outstation’s Parent Outstation

Each IEC 60870-5 Logical Outstation on a Geo SCADA Expert system represents a separate physical device or logical sector associated with an IEC 60870-5 Direct Outstation (see Configuring an IEC 60870-5 Outstation).

Use the Parent Outstation field on the Remote tab of the IEC 60870-5 Logical Outstation Form to specify the IEC 60870-5 database item that is the Logical outstation’s ‘parent’ outstation.

The 'parent' outstation can be one of the following:

Use the field’s browse button to display a Reference browse window and select the required IEC 60870-5 Direct Outstation from the window. (An IEC 60870-5 Direct Outstation can be the ‘parent’ for multiple IEC 60870-5 Logical Outstations.)

Be aware that should communications be lost with the parent outstation, Geo SCADA Expert will also lose communications with that outstation’s Logical outstations.


Disclaimer

Geo SCADA Expert 2021