Specify the Status Value Maps

Use the fields within the Status Value Maps section of the Value Maps tab to specify the Filtered Value Maps that store the input data for this slave outstation. The Filtered Value Maps that store a slave outstation’s data have to exist on your system before you can use the fields below to map to such data. (For more information, see Specify the Filtered Value Maps that Store the Source Data, and see Configuring Value Maps in the Geo SCADA Expert Guide to Core Configuration.)

Leave the fields blank for any Status Value Map types that are not used by this slave outstation.

For each Filtered Value Map that you specify, use the corresponding First IOA field to specify the address of the first input on that Value Map:


Disclaimer

Geo SCADA Expert 2021