Create and Configure a Report Control Block

The IEC 61850 standard defines a reporting mechanism using unsolicited data transmission. The report generation and transmission is controlled by a Report Control Block (RCB). A report control block contains all the necessary information required to generate a report such as the data set name, trigger options, and optional fields.

You use a Report Control Block database item to represent a Report Control Block in an IED from a substation with which Geo SCADA Expert is to interact using the IEC 61850 protocol.

The IEC 61850 Driver does not reserve the RCB before configuring and enabling it. Therefore, the IEC 61850 Driver may be incompatible with some servers which expect the RCB to be reserved first.

To create and configure a Report Control Block in the database:

  1. Right-click on the IED database item to display a context-sensitive menu. Select the Create or Update Data Sets and Report Control Blocks pick action generate the Report Control Blocks that are defined in the SCL file for the IED.
  2. Either collapse and expand the hierarchy or press F5 to refresh the database.
  3. Click on the IED database folder where you have created the Report Control Blocks database items.
    The Report Control Block database items that have been created are displayed.

The following properties are configured automatically:

You can edit the Data change, Quality Change, and Data Update options if required. The Integrity and General Interrogation options should always be the same as in the SCL file; the RCB Object is flagged with an error if these settings differ to those specified in the SCL file.

We recommend that you create the Report Control Block database item automatically, rather than manually. If you create the Report Control Block database item manually, you have to configure the properties manually. The configuration settings will be internally validated automatically and have to match the SCL file configuration. Else, you will get an error message, or the database item will not work.


Disclaimer

Geo SCADA Expert 2021