You can display User Query data in List form from the Queries Bar in ViewX or Virtual ViewX.
The procedure is as follows:
- Display the Queries Bar (see Display an Explorer Bar).
- Expand the User Queries branch.
 The tree structure expands to show the available User Queries.On a Virtual ViewX client, the branch is only available if your system is configured to allow mobile devices to access the Geo SCADA Expert database. 
- Double-click on the User Query you want to work with.
 The Filter Columns window is displayed.
- Use the Filter window to restrict the entries in the Queries List as required (see Filter a List).
- Select the OK button to apply any filters and to display the User Query data.
Further Information