Display a Queries List from the Queries Bar

To display a Queries List from the Queries Bar:

  1. Display the Queries Bar (see Display an Explorer Bar).
  2. Expand the System Queries branch if required.
    The tree structure expands to show the available Queries Lists. The entries vary, depending on the drivers that are installed on your system (some drivers support driver-specific Queries Lists, which are included if those drivers are installed)

    To display a Data Grid, Data Set, or Data Table's data in List format, expand the Data Grids, Data Sets, or Data Tables branch of the Queries Bar, respectively.
    You can expand the User Queries branch to display User Queries data in List format (see Display User Query Data). On a Virtual ViewX client, the branch is only available if your system is configured to allow mobile devices to access the Geo SCADA Expert database. (You cannot display User Queries in Original WebX.)

  3. Either:
    • Double-click on the type of Queries List that you want to display.

    or:

    1. Select the required type of Queries List.
    2. Press the ENTER key on the keypad.

    The Filter Columns window is displayed.

  4. Use the Filter Columns window to apply any filter settings as required (see Filter a List).
  5. Select the OK button on the Filter Columns window to apply any filter(s) and display the List.
    The relevant Queries List is displayed. The List contains entries for the items of the selected database type to which you have access and that match the filter criteria.

To display a List from the Queries Bar without first displaying the Filter Columns window, at step 3 above, either:

or:

  1. Select the entry for the Queries List that you want to display.
  2. Press the CTRL and ENTER keys simultaneously.

The relevant Queries List is displayed. The List shows all of the items of the selected database type to which you have access. For instance, if you select the Points entry, the List will include every point to which the currently logged on User Account provides access.

(If you select the Objects entry, the resultant List will include all of the database items—points, outstations, channels, Mimics, Groups, Logic Programs, and so on—to which you have access on your system.)


Disclaimer

Geo SCADA Expert 2021