Introduction to the MQTT Driver

This driver is an advanced driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring MQTT items and features in the Geo SCADA Expert database.

This guide also contains information for maintenance engineers.

Document Scope

This guide explains about the configuration, features and database items that are specific to Geo SCADA Expert's MQTT Driver.

WARNING

POTENTIAL SECURITY BREACH

We strongly recommend using network-connected Geo SCADA Expert drivers in a private network only (either physical or virtual). We recommend against using such drivers for communications over the public Internet. If the drivers are used over the public Internet, as a minimum those drivers should use valid SSL certificates to initiate secure connections and encrypt the data that is transmitted over the network.
Failure to follow these instructions can result in death, serious injury, or equipment damage. The breach in system security could expose sensitive data and the leave the database vulnerable to unauthorized and potentially malicious use.

MQTT is an ISO standard publish-subscribe-based messaging protocol. It is a lightweight protocol designed for communications between small sensors and mobile devices in remote locations, where network bandwidth is limited or unreliable.

The MQTT driver in Geo SCADA Expert supports communications using MQTT versions 3.1 and 3.1.1.

You run the MQTT driver in conjunction with the relevant MQTT extension driver. The extension driver enables Geo SCADA Expert to receive messages in the format that is supported by the MQTT clients that publish the messages. Use this guide in conjunction with the Geo SCADA Expert guide for that extension driver.


Disclaimer

Geo SCADA Expert 2021