Introduction to the MQTT JSON Schema A Driver

This driver is an extension driver. It provides additional application-specific functionality to the 'parent' driver with which it is associated. To interact successfully with devices using an extension driver, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring MQTT JSON Schema A driver items and features in the Geo SCADA Expert database.

The guide also contains information for maintenance engineers.

Document Scope

This guide explains the configuration, features and database items that are specific to Geo SCADA Expert’s MQTT JSON Schema A driver. The driver enables Geo SCADA Expert to retrieve data using either of two MQTT JSON Schema A message formats.

WARNING

POTENTIAL SECURITY BREACH

We strongly recommend using network-connected Geo SCADA Expert drivers in a private network only (either physical or virtual). We recommend against using such drivers for communications over the public Internet. If the drivers are used over the public Internet, as a minimum those drivers should use valid SSL certificates to initiate secure connections and encrypt the data that is transmitted over the network.
Failure to follow these instructions can result in death, serious injury, or equipment damage. The breach in system security could expose sensitive data and the leave the database vulnerable to unauthorized and potentially malicious use.

The MQTT JSON Schema A driver is an MQTT extension driver. It provides additional functionality to enable Geo SCADA Expert to retrieve data using either of two MQTT JSON Schema A message formats (see Supported Message Formats).

In order to retrieve data using the MQTT JSON Schema A message formats, Geo SCADA Expert needs to run both the MQTT driver and the MQTT JSON Schema A extension driver (see Confirm that the MQTT JSON Schema A Server Component is Installed).

Use this Geo SCADA Expert Guide to the MQTT JSON Schema A Driver alongside the Geo SCADA Expert Guide to the MQTT Driver. As much of the information in the latter guide is assumed knowledge, we recommend that you read the Geo SCADA Expert Guide to the MQTT Driver before reading this driver guide.


Disclaimer

Geo SCADA Expert 2021