Animations for Historic Data

You can add animated historic values to a Mimic. This is useful when you want a Mimic to show calculated values, such as the daily average value of a point.

To use historic data in an expression, you need to include the Historic properties of a point. For example, you could animate a text box to show the daily average of a point by using the following expression to animate the Value property:

"<point path and name>.Historic.ProcessedValue ('D-1D', 'D', 3)"

Where:

<point path and name> defines the location and name of the point for which you want to show historic data. Do not enter the angle brackets < >.

.Historic is the table that contains the point's historic values, and ProcessedValue is the historic value of the point. The remaining part of the expression defines the time scale and the type of calculation:

'D-1D' is the start time of the time range (resample interval). It is a time in the OPC Relative Time Format, and in this case is the start of yesterday (Start of Current Day - 1 Day = start of previous day).

'D' is the end time for the time range. Again it is a time in the OPC Relative Time Format. In this case, the end time is the start of the current day.

3 is the number that corresponds to the type of algorithm ('Average'). As an alternative to specifying the number of the algorithm, you can enter the algorithm's name enclosed between single quotation marks. This results in a more readable, but slightly less efficient, expression. The name of each algorithm appears in the Algorithm column in the table below. Use the table to determine whether the algorithm names comprise single words, multiple words with spaces, or are camel case (also known as 'medial capitals').

If the above expression used the algorithm name, rather than the algorithm number, it would appear as:

"<point path and name>.Historic.ProcessedValue ('D-1D', 'D', 'Average')"

You can also specify any custom historic algorithms that have been created on your system (see Historic Algorithms (Custom) in the Geo SCADA Expert Guide to Server Administration). With custom algorithms, you have to specify the algorithm name (as the numbers of custom algorithms are not visible).

Geo SCADA Expert only recalculates historic values when a point is updated. Therefore, a mimic may display false data if a point is not updated within a time range.

Take care with End and End Last Historic Algorithms used on clients, or with Geo SCADA Expert features, that run in Local Time with Daylight Saving Time. Ensure that the start and end times specified for the sample interval do not coincide exactly with the time at which the clock jumps backward. Include a small offset in the sample time, to offset the calculation to avoid the sample end or start time exactly matching the time that the clock jumps backward at the transition from Daylight Saving Time to Standard Time. A small offset of 1s or even 1ms should suffice. For more information about Daylight Saving Time, see The Effects of Daylight Saving Time Adjustments.

The built-in algorithms and their corresponding numbers are shown in the table below. You can access further information by clicking on the entry in the Algorithm column.

Number for Expression Algorithm Meaning

1

Interpolated

The interpolated value within the resample interval.

2

Total

The totalized value (time integral value) of the values in the resample interval.

3

Average

The mean average of the values in the resample interval.

4

Count

The number of raw values in the resample interval.

5

StdDev

The standard deviation of the values in the resample interval. This indicates how much the raw values in the resample interval deviate from the mean average values.

6

Min

The lowest value in the resample interval.

7

MinTime

The lowest value in the resample interval and the time stamp for the value.

8

Max

The highest value in the resample interval.

9

MaxTime

The highest value in the in the resample interval and the time stamp for the value.

10

Start

The value at the start of the resample interval. The timestamp is at the start of the interval.

11

End

The value at the end of the resample interval. The timestamp is at the end of the interval.

12

Delta

The difference between the first value and the last value in the resample interval.

13

Variance

The variance of the values in the resample interval. This indicates how much the raw values in the resample interval deviate from the mean average values.

14

Range

The difference between the minimum value and the maximum value in the resample interval.

15

DurGood

The amount of time (in seconds) for which the data in the resample interval is Good quality.

16

DurBad

The amount of time (in seconds) for which the data in the resample interval is Bad quality.

17

PerGood

The percentage of data in the resample interval that is Good (1=100%).

18

PerBad

The percentage of data in the resample interval that is Bad (1=100%).

19

Sum

The sum total of the values in the resample interval.

20

24hAverage

The average value during the previous 24 hours. The 24 hour period starts from the latest raw value.

21

8hAverage

The average value during the previous 8 hours. The 8 hour period starts from the latest raw value.

22

1hAverage

The average value during the previous hour. The hour period starts from the latest raw value.

23

Stepped

The stepped value. Typically, you would not use this algorithm in an expression as it returns the last value in the resample interval.

24

Min Last

The lowest last value in the resample interval. Last values are used when the resample interval contains null values—the last value is the previous raw value and it is used instead of a null value.

25

Max Last

The highest last value in the resample interval. Last values are used when the resample interval contains null values—the last value is the previous raw value and it is used instead of a null value.

26

Average Last

The average last value in the resample interval. Last values are used when the resample interval contains null values—the last value is the previous raw value and it is used instead of a null value.

27

Min Interpolated

The lowest interpolated value in the resample interval. Interpolated values are used when the resample interval contains null values—the interpolated value is the difference between the raw values and it is used instead of a null value.

28

Max Interpolated

The highest interpolated value in the resample interval. Interpolated values are used when the resample interval contains null values—the interpolated value is the difference between the raw values and it is used instead of a null value.

29

Average Interpolated

The average interpolated value in the resample interval. Interpolated values are used when the resample interval contains null values—the interpolated value is the difference between the raw values and it is used instead of a null value.

30

Time Average

A time-weighted average of the values in a resample. The Time Average algorithm takes into account the amount of time between value changes. Therefore, this average value is less influenced by a small number of unusual values. See Time Average.

31

End Last

The value at the end of the resample interval or the last value prior to the resample interval (if there are no values for the resample interval). The timestamp is the time at the end of the resample interval, even if the value returned was not reported during the time span for the resample interval.

32

Moving Range

The sum of the absolute differences between each pair of values in the resample interval.


Disclaimer

Geo SCADA Expert 2021