Using the Expression Window

You can use the Expression window to define a specific value for an animation property. You can also use it to enter a ViewX expression that defines a relationship between the animation property and a value in the database. For example, you can associate an animation property with the state of a digital point—the state of the digital point will affect the value for the animation property.

There are examples for the various animation properties in the animations sections. For example, for information on the Text Box animations and suitable entries, refer to Text Box Animations. A list of the animation sections is included at the start of the Animations section (see Animations).

To display the Expression window for an animation property, select an animation property on the Animations window and then select the Edit button. Alternatively, you can double-click on the required animation property on the Animation window.

The Expression window has 3 check boxes, and an expression text entry field that has a browse button feature:

Select the OK button to confirm your selections and close the Expression window.

Further Information

Expressions: see Understanding the Basics of Expressions in the Geo SCADA Expert Guide to Expressions.


Disclaimer

Geo SCADA Expert 2021