Introduction to the Mitsubishi Slave Driver

This driver is a simple driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring Mitsubishi Slave items and features in the Geo SCADA Expert database.

The guide also contains information of use to maintenance engineers.

Document Scope

This guide explains the configuration, features and database items that are specific to Geo SCADA Expert’s Mitsubishi Slave driver. The Mitsubishi Slave driver enables Geo SCADA Expert to act as a Mitsubishi MELSEC A PLC and report any data changes back to another Master (using the Mitsubishi MELSEC A protocol). The Slave transmits any changes to its database, or sets values or states in its database, upon request from its Master.

For information on how to configure Geo SCADA Expert to communicate with slave devices and PLCs using the Mitsubishi MELSEC A protocol, see the Geo SCADA Expert Guide to the Mitsubishi Driver.

The Slave can obtain its data directly from plant, from calculated values, or from any item in the Geo SCADA Expert database. Its Master can be another Geo SCADA Expert server, or a third party server that is using the Mitsubishi MELSEC A protocol.

The Mitsubishi Slave Driver provides extra functionality within a Geo SCADA Expert server for transmitting data or controlling points. A Mitsubishi Slave uses Value Maps for mapping point properties into memory, so that they can be accessed by the Mitsubishi MELSEC A protocol.

The Mitsubishi Slave documentation explains how to configure Mitsubishi Slave-specific features and items within the Geo SCADA Expert database (see The Transmission Protocol Supported by Geo SCADA Expert and see Configuring Mitsubishi Slave Devices in Geo SCADA Expert).

It also explains driver-specific aspects that may be of interest to system administrators and engineers when investigating unexpected behavior (relating to the Mitsubishi Slave driver) (see Mitsubishi Slave-Specific Status Display Attributes).

NOTE: There are no driver-specific pick actions for database items on this particular driver. However, users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions in the Geo SCADA Expert Guide to Core Configuration). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).


Disclaimer

Geo SCADA Expert 2021