Control VQT

Associated with: OPC UA Points on which controls are enabled

Security permission required to access this pick action: Control

You can use either the 'standard' Control pick action, or the driver-specific Control VQT pick action to write OPC UA point data to the current OPC UA server.

The Control VQT pick action differs from the Control pick action in that it enables you to write additional properties (the Quality and/or Timestamp) to the OPC UA server.

Select the Control VQT pick action to display the Control VQT window.

For each point type you can include one or more of the following:

To write a Value, Quality and/or Timestamp to the item, select the corresponding check box. Clear a check box to exclude that corresponding entry.

Select the OK button to write the selected data to the item on the OPC UA server.

Not all OPC UA servers support every combination of Value, Quality and Timestamp.

NOTE: If using this pick action with the Automation Interface, you have to specify the method name ControlVQT.


Disclaimer

Geo SCADA Expert 2021