OPC UA Subscriptions List

The OPC UA Subscriptions List is specific to the OPC UA driver - it is only available on systems on which that driver is installed. Like other Queries Lists, you can display the List from the Queries Bar. Alternatively, you can use the Display Subscriptions pick action to display a filtered list that just includes the OPC UA Subscriptions that reference a particular OPC UA Server.

The OPC UA Subscriptions List provides a summary of the status of the OPC UA Subscription database items to which your User Account and the client provide access.

As with other Lists, the OPC UA Subscriptions List consists of rows and columns. Each row represents an individual OPC UA Subscription and each column contains status information about that particular OPC UA Subscription item.

The OPC UA Subscriptions List contains these columns:

As with other Lists, you can right-click on an entry in the List to display a context-sensitive menu. From this menu, you can select options to display further information about an OPC UA Subscription, or perform various actions. For information about the actions that are specific to this type of database item, see Actions Associated with OPC UA Subscription Items.


Disclaimer

Geo SCADA Expert 2021