Introduction to the Pager Driver

This driver is a stand-alone driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported systems or devices. To interact successfully with such systems or devices, you need to:

Intended Audience

This guide is designed to be used by engineer-level users who are responsible for configuring the system and devices to communicate via the following protocols:

Document Scope

This guide explains how to configure and operate your Geo SCADA Expert system so that it can communicate with pager devices and mobile telephones.

In this Guide, we provide information about the Pager driver and explain how you can configure your Geo SCADA Expert system to utilize its features. When you have configured your Pager Services, Pager Channels, and User accounts as described, you will be able to use Geo SCADA Expert to send messages to pager devices and mobile telephones.

The information in the Pager Driver Guide is designed to provide you with information on the pager-specific properties that you will need to use when configuring your system to use the Pager Driver. For information on those properties that feature on Pager items and displays but are not specific to pagers, you should refer to the core (non-driver-specific) documentation.

If you are familiar with how the Pager Driver works and the protocols it supports, we recommend that you refer to Configuring Pager Devices in Geo SCADA Expert. There, you will find information on the various items you need to configure to allow the Pager Driver to send messages to pagers and mobile telephones.

When you have configured the necessary database items, you can use Geo SCADA Expert's actions to send messages manually. Alternatively, you can configure Geo SCADA Expert to send messages in response to alarms or periodically.


Disclaimer

Geo SCADA Expert 2021