Configure the General Realflo Analog Point Properties

Realflo Analog Input points are used to process gas, liquid or water flow calculation data in Geo SCADA Expert (see Configure Geo SCADA Expert to Monitor Realflo Calculation Data). (To process any other data on a Realflo controller, configure a ‘standard’ analog or digital point, rather than a Realflo Analog Input point.)

Use the fields at the top of the Analog Point tab on the SCADAPack Modbus Realflo Analog Input Point Form to configure the point’s common properties. Fields that are specific to Realflo Analog Input points are explained below. For properties that are also common to other points on the SCADAPack Modbus driver, see Configure Common Point Properties in the Geo SCADA Expert Guide to the SCADAPack Modbus Driver.

Examples:

In order to assess the amount of gas, liquid or water that has been used during the past month, you might configure a Realflo Analog Input point to have the following properties:

Source: Accumulation
Item: Flow volume in current month

In order to assess the current flow rate, you might configure a Realflo Analog Input point to have these properties:

Source: Flow Calculation
Item: Flow volume rate


Disclaimer

Geo SCADA Expert 2021