SCADAPack x70

Add and Configure the Entries in an IP Routing Table

You use a SCADAPack x70 IP Routing Table to specify the IP routing that a particular SCADAPack x70 device is to use in order to connect to a commercial TCP/IP network. You use the table to specify the packet forwarding and IP gateway services that are required to enable such functionality. You can specify up to 20 static IP routes per IP Routing Table.

Where TCP/IP packets are routed through the SCADAPack x70 device, IP routes may or may not be needed depending on the Disable IP Forwarding configuration (see Enable or Disable IP Forwarding):

Where the SCADAPack x70 device is directly communicating using an IP address in the same local subnet as one of its interfaces, an IP route is not required, regardless of the Disable IP Forwarding configuration.

Where IP route entries are added with overlapping subnets, the IP route entry with the narrowest subnet is the entry used to route the data packet. This establishes a selection priority among multiple IP routes. Where multiple routes could be applied to the same IP address, the route to be used is chosen in the following order:

  1. Host route (subnet mask 255.255.255.255).
  2. Narrowest subnet Network route (for example, subnet mask 255.255.255.252).
  3. Gateway route (where a gateway IP is configured on the route).
WARNING

communication loss

Omission of IP routes that are used by Geo SCADA Expert can lead to loss of communication between Geo SCADA Expert and your SCADAPack x70 device. Similarly, omission of IP routes that are used by other devices with which the SCADAPack x70 device is expected to communicate can lead to loss of communication between the SCADAPack x70 device and those devices.
Verify that the required IP routes are included in the IP Routing Table and that the specified settings are valid for the device and your network.
Failure to follow these instructions can result in death or serious injury.

The entries that you specify in an IP Routing Table are persistent (that is, they are retained when the SCADAPack x70 device restarts).

In the Geo SCADA Expert database, the table is built into the SCADAPack x70 Device Configuration item to which it relates. Changes made to the routing configuration are downloaded to the SCADAPack x70 device when that device's Download Configuration pick action is next executed.

 

You specify these properties for each route in a SCADAPack x70 IP Routing Table:

Destination Address

The IP address of the device or sub-network in the remote network to which the SCADAPack x70 device is to transmit TCP/IP packets. Use the Destination Address in conjunction with the Subnet Mask to identify either a single host address, or a range of target host IP addresses.

 

192.186.1.0

Subnet Mask

Used in conjunction with the Destination Address to identify either a single host address, or one of a range of host addresses (a subnet) to which the SCADAPack x70 device is to transmit TCP/IP packets.

 

255.255.255.0

Destination Port

The physical port on the SCADAPack x70 device via which that device is to transmit the TCP/IP packets.

When adding or editing a route, you use a combo box to select the required port. The options that are available vary, depending on the model of SCADAPack x70 device and its configuration, but might include Ethernet Port and/or Serial Port entries.

Serial Port options are only available if the SCADAPack x70 device has one or more serial ports on which the Port Function is set to 'PPP/TCPIP' (see Device Configuration Serial Port Tabs).

Gateway IP Address

The IP address of the host that provides the ‘gateway’ to the target host.

 

192.168.0.1

The Gateway IP Address should be on the same subnet as the SCADAPack x70 device’s interface for the corresponding route. For example, if the Ethernet 1 interface is configured with an IP address of 192.168.0.1 and a subnet mask of 255.255.255.0, the gateway address could be 192.168.0.2, but should not be 192.169.0.1

Metric

Defines the route priority, or cost, of an interface when multiple paths exist for interconnecting IP Hosts. The higher the number, the lower the priority. Set the entry to zero to apply the default metric value ('cost') for a particular type of route. Generally, PPP interfaces tend to have a higher metric, and therefore a lower priority, than Ethernet interfaces.


Disclaimer

Geo SCADA Expert 2021