SCADAPack x70

Create Protocol Point

Associated with: SCADAPack x70 Analog, Digital, and Counter Configuration items

Security permission required to access this pick action: Configure

Use the Create Protocol Point pick action to create a SCADAPack x70 Point of the relevant point- and protocol-type and automatically associate it with the selected SCADAPack x70 Analog, Digital, or Counter Configuration item. The newly created Point might require some additional configuration (see Minimum Configuration - Points), but the majority of its properties will be assigned default values where possible.

The pick action is only available on a SCADAPack x70 Analog, Digital, or Counter Configuration item that:

The pick action is no longer available on the Configuration item once it has a SCADAPack x70 Point associated with it for that particular communications protocol.

The pick action is particularly useful on systems that use Group Templates and Group Instances. It enables the rapid creation of protocol-specific Points in all of the Group Instances that reference the Group Template in which the pick action is being used.

To create a protocol-specific Point for the selected SCADAPack x70 Analog, Digital, or Counter Configuration item:

  1. Ensure that:
    • The SCADAPack x70 Configuration item has a suitable name. (As the same name will be used as the basis for the name of the protocol-specific Point that is created using the Create Protocol Point pick action (see below for more information).)
    • The protocol-specific content is suitably set up on the SCADAPack x70 Configuration item, including (if applicable) the configuration that indicates whether the Configuration item relates to an input or output. This latter information is important, as it determines whether the pick action creates an Input Point or an Output Point.
      The protocol-specific properties are typically on the <Protocol Type> tab of the configuration Form.
  2. From the SCADAPack x70 Configuration item's context-sensitive menu, select the Create Protocol Point pick action.
    The Create Protocol Point window is displayed.

  3. Use the Protocol field to select the required communications protocol for the SCADAPack x70 Point that is to be created and associated with the SCADAPack x70 Configuration item. You are only provided with the names of the protocol(s) with which the SCADAPack x70 Configuration item is already configured to communicate. This is currently restricted to the DNP3 protocol. (If the required option is not there, cancel the pick action and check the item's configuration; in particular the configuration on the relevant <Protocol Type> tab.)

  4. Select the OK button to confirm your selection and trigger Geo SCADA Expert to create the SCADAPack x70 protocol-specific Point and associate it with the Configuration item. The Point will be placed in the same Group as the Configuration item (you might need to close and reopen the Group in the Database Bar in order to refresh that Explorer Bar so that it shows the newly created Point). The protocol-specific Point will automatically be associated with the Configuration item from which the pick action was triggered.

  5. Edit the configuration of the newly created SCADAPack x70 protocol-specific Point as required. A message area at the bottom of the Point's configuration Form will display messages relating to any invalid, incomplete, or conflicting configuration that requires addressing. For more information, see Mandatory Configuration and Invalid Configuration Messages in the Geo SCADA Expert Guide to Core Configuration, and see the point configuration topics for the relevant communications protocol in this driver guide.


Disclaimer

Geo SCADA Expert 2021