SCADAPack x70

Number of Modbus Scanner Objects

Associated with: SCADAPack x70 Device Configuration items.

The Number of Modbus Scanner Objects status attribute indicates the number of SCADAPack x70 Modbus Point Scanner items that are associated with the selected SCADAPack x70 Device Configuration item. You use this status attributeto determine the number of Modbus Point Scanner items that are currently associated with, and/or can still be associated with, the SCADAPack x70 Device Configuration item within the given limit. If there are no associated Modbus Point Scanner items, the status attribute displays the value '0'.

For information about Modbus Point Scanners, see Configure a Modbus Point Scanner.


Disclaimer

Geo SCADA Expert 2021