SCADAPack x70

Points and Configuration Items Supported by the Driver

The SCADAPack x70 driver differs from other Geo SCADA Expert drivers in that you configure an 'object-pair' of database items to represent a single item of I/O with which Geo SCADA Expert is to interact on a SCADAPack x70 device. This includes I/O that is built into the device, plugged into the device, or that exists on another device or elsewhere on the system and for which a SCADAPack x70 device provides data concentrator functionality.

For each item of I/O for which Geo SCADA Expert is to interact, you need to configure:

From a day-to-day operational point of view, you interact only with the SCADAPack x70 protocol-specific ('Point') database items. These are the only driver items that:

  • raise alarms and generate events
  • store the points' values
  • provide pick actions that enable you to interact with the points
  • need appear on Mimics.

(You purely use the SCADAPack x70 Configuration items to store and download properties to the SCADAPack x70 devices; thereafter you use the SCADAPack x70 protocol-specific Point items to store and process the points' data and interact with the points on a day-to-day operational basis.)

 

The driver supports the following types of SCADAPack x70 Configuration items:

 

If Geo SCADA Expert or another SCADA master is to communicate with the SCADAPack x70 devices using the DNP3 protocol, you also need to configure the relevant types of point for that protocol. For DNP3 communications, the driver supports these types of SCADAPack x70 Point:

 

To create and configure any of the above database items, you have to be logged on with a User Account that has the Configure Database feature enabled and the relevant permissions set (see Overview of User Account Security in the Geo SCADA Expert Guide to Security).

You configure the database items by editing the properties on the item's Form (see Display a Form in the Geo SCADA Expert Guide to Core Configuration). When each item is created in the database, many of its configuration properties are assigned default values—you only need to edit such properties if different values are required. For information on which properties you need to configure as a minimum in order to produce a functional database item, see the 'Minimum Configuration' topics in this guide.


Disclaimer

Geo SCADA Expert 2021