Introduction to the Schneider Electric Rod Pump Controller Driver

This driver is an extension driver. It provides additional application-specific functionality to the 'parent' driver with which it is associated. To interact successfully with devices using an extension driver, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring Schneider Electric Rod Pump Controller (SE RPC) driver items and features in the Geo SCADA Expert database.

The guide also contains information for operators and engineers who use the Schneider Electric Rod Pump Controller driver to monitor rod pump activity.

Document Scope

This guide explains the configuration, features and database items that are specific to Geo SCADA Expert’s Schneider Electric Rod Pump Controller driver. The Schneider Electric Rod Pump Controller (SE RPC) driver is an Advanced Modbus extension driver. It provides additional functionality to enable Geo SCADA Expert to interface with Schneider Electric rod pump controllers. Using the driver, Geo SCADA Expert can upload rod pump and other data from the controllers. The uploaded dynacard data can then be displayed as a series of Dynagraphs that users can analyze to determine the effectiveness of the pumps in the well fields.

ATTENTION: Throughout this guide, mentions of the 'Schneider Electric Rod Pump Controller driver' are abbreviated to 'SE RPC driver' ; similarly, 'Schneider Electric Rod Pump Controller' is abbreviated to 'SE Rod Pump Controller'.

In order to communicate with Schneider Electric rod pump controllers, Geo SCADA Expert needs to run both the Advanced Modbus driver and the Schneider Electric Rod Pump Controller extension driver (see Confirm that the SE RPC Server Component is Installed).

Use this Geo SCADA Expert Guide to the Schneider Electric Rod Pump Controller Driver alongside the Geo SCADA Expert Guide to the Advanced Modbus Driver. As much of the information in the latter guide is assumed knowledge, we recommend that you read the Geo SCADA Expert Guide to the Advanced Modbus Driver before reading this driver guide.

The Schneider Electric Rod Pump Controller driver documentation explains how to:

It also explains features that are of interest to operators, such as:

System administrators and engineers who are investigating unexpected behavior relating to the SE RPC driver might wish to refer to the following sections:

For further information on Schneider Electric rod pump controllers, or on analyzing rod pump data, please refer to the documentation provided with the Schneider Electric rod pump controllers and well field equipment.


Disclaimer

Geo SCADA Expert 2021