Operands and Resulting Data Types
This topic lists the data types that the various SQL operators support, along with the data type that is returned by the operation. Use this topic in conjunction with the generic topic on Operators and the topics that are specific to the different types of operators. Links to the latter topics are provided below each table.
IN operator
With this logical operator, all of the values that you include in an array must be of the same data type.
| Data Type that you can include in the array | 
|---|
| 32-bit Integer | 
| 64-bit Integer | 
| Real | 
| Boolean | 
| String | 
| DateTime | 
| Interval | 
| Location | 
For more information, Conditions.bool-primary-in.
Numeric Negation operator
This is a unary operator, where both operands have to be of the same data type.
| Data Type of Operands | 
|---|
| 32-bit Integer | 
| 64-bit Integer | 
| Real | 
| Interval | 
NOT Negation operator
| Data Type of Operand | 
|---|
| Boolean | 
Do not confuse the NOT operator with the NOT condition. You can use the NOT condition to inverse the logic of an SQL condition. For example, NOT EXISTS, NOT BETWEEN, NOT IN, and so on. For more information about the NOT condition, see Conditions.
De-reference operator
| Data Type of Operands | 
|---|
| Reference | 
| Aggregate | 
For more information, see de-reference operator.
Multiplication, Division, and Concatenation operators
| Data Type of First Operand | Operator | Data Type of Second Operand | Resulting Data Type | 
|---|---|---|---|
| 32-bit Integer | * | 32-bit Integer | 32-bit Integer | 
| 32-bit Integer | * | Real | Real | 
| 64-bit Integer | * | 64-bit Integer | 64-bit Integer | 
| 64-bit Integer | * | Real | Real | 
| Real | * | 64-bit Integer | Real | 
| 64-bit Integer | * | 32-bit Integer | 64-bit Integer | 
| 32-bit Integer | * | 64-bit Integer | 64-bit Integer | 
| Real | * | 32-bit Integer | Real | 
| Real | * | Real | Real | 
| 32-bit Integer | * | Interval | Interval | 
| 64-bit Integer | * | Interval | Interval | 
| Real | * | Interval | Interval | 
| Interval | * | 32-bit Integer | Interval | 
| Interval | * | 64-bit Integer | Interval | 
| Interval | * | Real | Interval | 
| 32-bit Integer | / | 32-bit Integer | 32-bit Integer | 
| 64-bit Integer | / | 64-bit Integer | 64-bit Integer | 
| 64-bit Integer | / | 32-bit Integer | 64-bit Integer | 
| 32-bit Integer | / | 64-bit Integer | 32-bit Integer | 
| 32-bit Integer | / | Real | Real | 
| 64-bit Integer | / | Real | Real | 
| Real | / | 32-bit Integer | Real | 
| Real | / | 64-bit Integer | Real | 
| Real | / | Real | Real | 
| Interval | / | 32-bit Integer | Interval | 
| Interval | / | 64-bit Integer | Interval | 
| Interval | / | Real | Interval | 
| String | || | String | String | 
| Bit String | || | Bit String | Bit String | 
For more information, see Expressions.expr-term.
Addition and Subtraction operators
| Data Type of First Operand | Operator | Data Type of Second Operand | Resulting Data Type | 
|---|---|---|---|
| 32-bit Integer | + | 32-bit Integer | 32-bit Integer | 
| 32-bit Integer | + | Real | Real | 
| 32-bit Integer | + | 64-bit Integer | 64-bit Integer | 
| 64-bit Integer | + | 64-bit Integer | 64-bit Integer | 
| 64-bit Integer | + | 32-bit Integer | 64-bit Integer | 
| 64-bit Integer | + | Real | Real | 
| Real | + | Real | Real | 
| Real | + | 32-bit Integer | Real | 
| Real | + | 64-bit Integer | Real | 
| DateTime | + | Interval | DateTime | 
| Interval | + | DateTime | DateTime | 
| Interval | + | Interval | Interval | 
| 32-bit Integer | - | 32-bit Integer | 32-bit Integer | 
| 32-bit Integer | - | Real | Real | 
| Real | - | 32-bit Integer | Real | 
| 64-bit Integer | - | 64-bit Integer | 64-bit Integer | 
| 64-bit Integer | - | 32-bit Integer | 64-bit Integer | 
| 32-bit Integer | - | 64-bit Integer | 64-bit Integer | 
| 64-bit Integer | - | Real | Real | 
| Real | - | 64-bit Integer | Real | 
| Real | - | Real | Real | 
| DateTime | - | DateTime | Interval | 
| DateTime | - | Interval | DateTime | 
| Interval | - | Interval | Interval | 
For more information, see Expressions.expression.
Comparison operators
The valid operand data types for the comparison operators =, <>, <, >, <=, and >= are as follows. In each case, the result is Boolean.
| Data Type of First Operand | Data Type of Second Operand | 
|---|---|
| 32-bit Integer | 32-bit Integer | 
| 32-bit Integer | 64-bit Integer | 
| 64-bit Integer | 32-bit Integer | 
| 64-bit Integer | 64-bit Integer | 
| 32-bit Integer | Real | 
| 64-bit Integer | Real | 
| Real | 32-bit Integer | 
| Real | 64-bit Integer | 
| Real | Real | 
| Boolean | Boolean | 
| 32-bit Integer | Boolean | 
| 64-bit Integer | Boolean | 
| Boolean | 32-bit Integer | 
| Boolean | 64-bit Integer | 
| String | String | 
| Binary | Binary | 
| DateTime | DateTime | 
| Interval | Interval | 
| Location | Location | 
| Location | String | 
| String | Location | 
For more information, see Conditions.bool-primary-comparison.