Welcome to the Geo SCADA Expert Guide to Working with SQL

Welcome to the Geo SCADA Expert Guide to Working with SQL. This guide is designed for use by engineers that have SQL programming experience. This is not a comprehensive guide to SQL, but provides generic information about the use of key aspects of SQL and a technical reference for the SQL features that are supported in Geo SCADA Expert. For more information about SQL, see Implementation of SQL in Geo SCADA Expert.

Geo SCADA Expert uses a custom SCADA-orientated revision of SQL, with the addition of some custom syntax, which is documented in the relevant sections where it is used.

Intended Audience

This guide is designed to be used by engineers who are responsible for creating SQL queries in Geo SCADA Expert.

Document Scope

This guide provides guidelines for the general use of SQL queries with your Geo SCADA Expert software solution. The most common SQL operation in Geo SCADA Expert is the query that allows you to access and display data from the database. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

SQL queries should be written by engineers who have the appropriate experience and knowledge of the SQL language. Running a badly designed SQL query can have an adverse affect on the system. All queries should include suitable restrictions to limit the number of records that are retrieved from the database. An SQL query that queries large amounts of data will affect the performance of the server while that query executes.

Further Information

Requirements when Querying Historic Tables.

Specify Whether the Guest User can Execute SQL Queries.

SQL Query and List Problems in the Geo SCADA Expert Guide to the Server Status Tool.

Inefficient SQL Queries in the Geo SCADA Expert Guide to the Server Status Tool.

Avoid using the underscore character ( _ ) in the names of database items: see Naming Restrictions in the Geo SCADA Expert Guide to Core Configuration.

Designing Queries for GIS Map Markers in the Geo SCADA Expert Guide to Mapping and Geographic Information.


Disclaimer

Geo SCADA Expert 2021