Designing Queries for GIS Map Markers

As a simpler alternative to specifying the SQL query within a Map Set hyperlink, you can use a User Query database item. You can configure the User Query to hold a database query of Geo SCADA Expert database items that are to be displayed on maps. When configured, the context-sensitive menu for the User Query database item will include a Display Query Results option. You can use this menu option to display the query results in a list, which is useful for testing the SQL query. Each individual entry within the SQL query list should translate to a Map Marker when shown on a map, although entries with the same location will appear superimposed over each other, obscuring the view of some markers. Data referred to by the SQL query will update whenever the map moves, or at a rate of once per minute.

You can use the following SQL column names to define the behavior of the Map Marker:

In order to display the assets on a map, the SQL queries that are within hyperlinks need to contain the following columns as a minimum:

The above columns are parsed based on Name rather than Attribute, allowing for color animations to be customized as required. You can configure the ToolTip to contain HTML formatting codes.

 

The following map hyperlink uses the AlarmSetCount, AlarmAcceptedCount and AlarmClearedCount variables on the CGroup table to manipulate the Foreground color, adjusting the color used to display the associated map icon for each Group. The ordering of the result set causes the assets with active alarms to display on top of those without, if there is any overlap.

SELECT FULLNAME, FULLNAME || '<br>Highest_Severity:_' || AlarmSeverityDesc as "TOOLTIP", GISLOCATION->LATITUDE, GISLOCATION->LONGITUDE,

CASE WHEN AlarmSetCount > 0 THEN 255

WHEN AlarmAcceptedCount > 0 THEN 255

WHEN AlarmClearedCount > 0 THEN 150*256 ELSE 0 END AS "Foreground", Background,

CASE WHEN AlarmSetCount > 0 THEN 1 ELSE 0 END AS "Blink", AlarmSetCount, AlarmAcceptedCount, AlarmClearedCount

FROM CGROUP

ORDER BY AlarmSetCount, AlarmAcceptedCount, AlarmClearedCount

 

This example results in the display containing a smooth range of colors, as the Map Marker's foreground color is based on the value of a point that is associated with a group’s location:

SELECT g.Id as "Id", g.FullName as "FullName",

g.FullName || '<br>Value: ' || FormatValue (r.Walk Using '0.00') as "Tooltip",

g.GISLOCATION->LATITUDE as "GISLOCATION->LATITUDE", g.GISLOCATION->LONGITUDE as "GISLOCATION->LONGITUDE",

case

when r.Walk < 50 then (cast(r.Walk/100*2*255 as INT) + 255*256)

when r.Walk > 50 then (255 + cast( (100-r.Walk)/100*2*255 as INT)*256)

end as "Foreground",

255+256*255+256*256*255 as "Background", 0 as "Blink"

FROM CGROUP AS g left join CRandom as r on r.ParentGroupId = g.Id

WHERE g.FULLNAME LIKE 'Sites.%'

Aliases

Query column names are not case-sensitive, and should not contain the table name or alias; therefore, a column alias should be used if more than one table is referenced in the query.

If you are using table alias names, then you must also use an alias for the column.

 

If you use this table alias name:

FROM CGROUP AS g

Then you must also use an alias for the column:

g.GISLOCATION->LATITUDE as "GISLOCATION->LATITUDE"

It is important that you use the AS keyword for table and column aliases. While it can be omitted and the query will still work, the keyword must be present in order for the map to parse the query.

Spacing

Take care with spacing between:

Ensure that there is only one space (or a single new line) between each of the above clauses and column or table names.

You can check the database server log to see how the query has been interpreted and modified.

Linked Tables and Nested SELECTs

The query used by the map display is altered automatically by the map code. This is to limit the data that the query retrieves, because the markers are outside the bounds of the display.

 

The following additional WHERE clause is added, and if there is an existing WHERE clause it is added with an additional AND keyword:

WHERE (GEOPOSITION WITHIN REGION '5.05811437435571,-95.017822265625' TO '-5.05811437435572,-60.982177734375' )

When using data from external Geo SCADA Expert databases, you may need to use a nested SELECT.

 

SELECT * FROM ( SELECT TOP (5000)

A.FULLNAME, B.LATITUDE AS "GISLOCATION->LATITUDE", B.LONGITUDE AS "GISLOCATION->LONGITUDE"

FROM

ODBC_GROUP AS A JOIN ODBC_TEST AS B ON A.ID = B.ID

WHERE (A.GISLOCATIONSOURCE = True)

)

You should structure your query slightly differently if either of the following scenarios applies:

With either scenario, you may want to alter the query to prevent the additional WHERE clause from being added. Do this by including an additional WHERE clause within a nested SELECT, although this will affect performance because the map will query all rows. There is a limit of 5000 records in map queries, which will apply in this case.

For more information about custom tables, see Custom Tables - An Overview.

Sorting

Map markers are drawn from the start of the results to the end of those results. By using an ORDER BY clause you can control which markers appear on top. You may want to take advantage of this to display significant locations last, such as those indicating alarm states.

Further Information

Associating User Queries with a Map Set.

Working with SQL: see the Geo SCADA Expert Guide to SQL.

Creating a Hyperlink to a Map.

GISLOCATION: see Expressions.expr-primary-location, also see de-reference operator and Geospatial Index in the Geo SCADA Expert Guide to SQL.

GEOPosition: see Expressions.expr-primary-region and see Expressions.expr-primary-location in the Geo SCADA Expert Guide to SQL.


Disclaimer

Geo SCADA Expert 2021