Users List

You can use ViewX or Virtual ViewX to display the Users List. The Users List is an SQL based Queries List that contains information about some or all of the user accounts on your system (depending on the filtering that is applied).

The Users List is useful when you need to view and compare information for user accounts, for example, if you need to find out when the user accounts in a specific Group need to have new passwords configured. (For information about a specific user account, you can view that user account's Status display (see Status Attributes Associated with User Accounts).)

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

A User Pattern is not an actual configured or built-in user, so it will not be included in any Users Lists. To display a list of the User Patterns that exist in your database (and to which you have access), display the Objects List and set the filter Type (TypeDesc) to User Pattern. For more information, see Display a Queries List from the Queries Bar, and see Add a Filter to a List.

Further Information

For more information on using Queries Lists, please refer to the Geo SCADA Expert Guide to Lists.


Disclaimer

Geo SCADA Expert 2021