Installing Windows Performance Monitor Counters

Geo SCADA Expert includes a set of custom counters that you can install in the Windows Performance Monitor to provide information about the performance of your Geo SCADA Expert database.

To install the Geo SCADA Expert counters, use the counter registration tool provided within Windows as follows:

  1. Open a Command Prompt window in Microsoft Windows®.
  2. Use the cd command to change the directory to that in which the Geo SCADA Expert Performance Monitor Counter file is installed. The Tool is installed in the same directory as other Geo SCADA Expert installation files. The default location of these files varies depending on the Windows operating system (see File Locations (Default) in the Geo SCADA Expert Installation Guide).

    Example:

    If Geo SCADA Expert is installed at the default location on a machine that is running Windows 10, you would enter:

    cd c:\program files\Schneider Electric\ClearSCADA

  3. Press the Enter key.
  4. Use the dir command to check that the Geo SCADA Expertcounter file (DBKernal.man) is present.

  5. Register the performance counters by entering the following at the command prompt:

    lodctr /M:DBKernel.man

ATTENTION: Registering performance counters should not adversely affect the performance of the server, however third-party tools such as PerfMon.exe that access and plot the data could degrade system performance if excessive numbers of plots of counters are enabled.

When the counters have been successfully registered you can use the Using Windows Performance Monitoring Counters to analyze your system.


Disclaimer

Geo SCADA Expert 2021