Start and Stop a Driver

You can use the Geo SCADA Expert Server Status Tool to start and stop a driver. This may be necessary when:

To start, stop, or restart a driver:

  1. Run the Geo SCADA Expert Server Status Tool (see Run the Server Status Tool in the Geo SCADA Expert Guide to Server Status).
  2. Log on if required, and then expand the General branch, and select Modules.
  3. Right-click on the driver that you want to start, stop, or restart to display a context sensitive menu.
  4. Select the relevant option:
    • Start—To start the driver. The driver will run and will re-establish its software connections.
    • Stop—To stop the driver. The driver will stop running and will release its software connections.
    • Restart—To stop the driver, and then start it again.
    • Automatic—The driver will start automatically as long as there are items for that driver in the database (the driver’s Object entry has to be above 0). When the driver starts automatically, it runs and re-establishes its software connections without any user interaction.
    • If the database does not contain any items for a driver that is set to autostart, the driver will be unable to start automatically (even if configured to do so). This is a precautionary measure to stop unused drivers from accessing system resources.

When you are familiar with the start, stop, and restart techniques, you can proceed to learn how to Alarm Limits.


Disclaimer

Geo SCADA Expert 2021