Run the Server Status Tool

The Server Status Tool contains statistical and diagnostic information that you can use to assess your system and investigate unexpected system behavior.

To run the Server Status Tool:

  1. On the Geo SCADA Expert server, right-click on the Geo SCADA Expert Server icon in the Windows taskbar.

    A context-sensitive menu is displayed.

  2. Select the Status option.
    The Server Status Tool is displayed. Depending on the way your system is configured, you may be able to browse the groups of categories immediately or you may be prompted to log on via your User account (use the same Username and Password that you would use to log on to ViewX)

    In order to log on to the Server Status Tool successfully, your User Account has to be assigned the System Admin security permission.

Alternatively, access the Server Status Tool as follows:

  1. In Windows, select the Start menu. Scroll down the alphabetical list of installed applications and expand the EcoStruxure Geo SCADA folder.
  2. Select the Server Status option.
    The Geo SCADA Expert Server Status Tool is displayed.

Alternatively, you can also access the Server Status Tool from the ViewX ribbon, as follows:

  1. Launch the Geo SCADA Expert ViewX.
  2. On the ViewX ribbon, double-click the Server Status icon.
    The Geo SCADA Expert Server Status Tool is displayed.

If you are unfamiliar with the Server Status Tool, see Overview of the Server Status Tool.

If you are familiar with the Geo SCADA Expert Status Tool, refer to the section you require:


Disclaimer

Geo SCADA Expert 2021