OPC Status Information

The Server Status Tool provides status information that is organized into groups of categories, each of which contains sub-categories. One of these groups is named OPC.

The OPC group provides status information about the OPC tags that are being used by clients connected to the server. For example, a client that is displaying a Mimic with ‘live’ values will reference an OPC tag for each value. Information about each of those tags is shown in the OPC group on the Server Status Tool (on the server to which the client is connected).

The OPC group contains the following sub-categories:


Disclaimer

Geo SCADA Expert 2021