System Architectures

The first stage of the server configuration is to define the type of system architecture to which the server belongs. You can use the Server Configuration Tool’s Partners settings to configure the server so that it recognizes the structure of your system and can interact with any other servers. To do this, you should have an understanding of the various server architectures and server connection and monitoring features.

The following sections describe the available server architectures and explain how the servers synchronize and interact with each other. Information is provided on each of the server features that you can configure in the Partners settings:

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Multi-server systems (redundancy) are only supported by full versions of Geo SCADA Expert. You can find information about the version you have installed by running ViewX and selecting Help>About.

For information on using a Geo SCADA Expert system with Remote Desktop applications, see Geo SCADA Expert on Citrix and Remote Desktop Services.


Disclaimer

Geo SCADA Expert 2021