Working with the Server Status Tool

To help you monitor your system and investigate unexpected system behavior, Geo SCADA Expert includes a Server Status Tool. Available on your Geo SCADA Expert servers, the Server Status Tool provides detailed statistical and diagnostic information.

Using the information shown in the Server Status Tool, you can:

In this section, we provide an Overview of the Server Status Tool. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

When working with the Server Status Tool, you will also need to be familiar with the Server Status Categories.

You can also use the OPC Data Bar to view status values, see Working with the OPC Data Bar.


Disclaimer

Geo SCADA Expert 2021