Server Status Categories

The Server Status Tool provides status information that is organized into the following categories:

If you select the folder for a branch of status categories (rather than select a specific category from within that branch), the tool will display the status information that relates to the first category in that branch. For example, if you select the folder for the Server branch, the tool will display the status data for the Advise Threads category (as that is the first category in the Server branch).


Disclaimer

Geo SCADA Expert 2021