Introduction to the Sofrel Driver

This driver is an advanced driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring Sofrel items and features in the Geo SCADA Expert database.

The guide also contains information for:

Document Scope

This guide explains the configuration, features and database items that are specific to Geo SCADA Expert's Sofrel driver.

The Sofrel driver supports two Modbus transport protocols:

Sofrel outstations do not support Modbus RTU over TCP or UDP directly, so this would only be used when communicating via a 'Modbus gateway' device.

In addition the driver enables Geo SCADA Expert to communicate with devices using two Sofrel protocols:

The driver supports the following Sofrel outstation models:

The Sofrel driver allows interoperability between RTUs (Remote Terminal Units) and Geo SCADA Expert. A Sofrel network typically consists of a single Geo SCADA Expert master and multiple outstations.

Most Sofrel outstations can support up to four masters, refer to the Sofrel literature for more information.

The Geo SCADA Expert master maintains a local database that holds a copy of the data stored in each outstation.

Geo SCADA Expert processes the data received from the outstation and:

The data sent by an outstation may be:

One of the fundamental concepts of Sofrel is that an outstation can buffer historic data. The outstation sends its buffered data to Geo SCADA Expert when it sends a poll request to the outstation—these can be scheduled by Geo SCADA Expert to optimize use of the communications network.

Geo SCADA Expert supports 'report data' from the S50 range of outstations, which is a specialized form of historic data used for daily reporting.

Alternatively, the outstation can dial-in (PSTN/GSM) or make a connection (Network) to report alarms.

This guide explains how to configure Sofrel specific features and items within the Geo SCADA Expert database.


Disclaimer

Geo SCADA Expert 2021