Web Server Ports Configuration

This page of the Installation Wizard is only displayed on a Geo SCADA Expert server installation. (It is not displayed on a client-only installation.)

This page is not shown when you modify an existing installation. To change the Web Server Port settings on an existing installation, use the IIS Manager application to change the settings and then replicate any changed port settings in the WebX section of the Server Configuration Tool.

A local IIS reverse proxy is now installed and configured as part of the Geo SCADA Expert installation when you use the Installation Wizard to install the server components. We recommend that you use this local IIS reverse proxy to perform TLS negotiation on behalf of the Geo SCADA Expert server.

Use the Web Server Ports Configuration page to specify Geo SCADA Expert's web server port and the ports that the IIS reverse proxy is to use. Also specify the certificate that the IIS reverse proxy is to use for HTTPS communications. The properties on this page are used to configure the local proxy settings in the Internet Information Services (IIS) Manager application.

The settings in the WebX section of the Server Configuration Tool are used to inform the Geo SCADA Expert server of the current IIS configuration. These are initially set up to use the settings that you specify above. If the settings are later changed in the IIS Manager application, remember to also update the settings in the WebX section of the Server Configuration Tool. For more information, see Configuring Security and Connection Settings for Original WebX Clients.

Once you are ready to move onto the next stage of the installation process. select the Next button to go to Ready to Install.


Disclaimer

Geo SCADA Expert 2021