Numeric Point Configuration

The Totalflow Numeric point is by default an Analog type point.

For information on Analog Point Formatting, see Define the Appearance of an Analog Point’s Values in the Geo SCADA Expert Guide to Core Point Configuration.

Use the Historic tab to define data storage properties for a point (see Defining Historic Details for a Point in the Geo SCADA Expert Guide to Core Point Configuration). This tab is only displayed for points that can support historic data.

The Totalflow-specific configuration settings for the Totalflow Numeric Point object are mainly on the Options tab. A few settings on the Control tab are also discussed below. For information, see:

Further Information

Defining Analog Point Details

Tabs on Point Forms


Disclaimer

Geo SCADA Expert 2021