The XAXIS section in a TrendSpec definition has to have one mandatory value, <X-Axis Mode>.
| Mandatory Value | Type | XAXIS Mandatory Values | 
|---|---|---|
| Comments | ||
| <X-Axis Mode> | Identifier value | Use to define the type of time scale used for the x-axis. Specify one of these values: Absolute, RelativeNow, or RelativeLatest. (For information on each type of x-axis mode, see Configure the X-Axis.) 
                                        Example:
                                     RelativeLatest | 
If required, you can specify one or more XAXIS Optional Values after the above mandatory value.