Specify any optional XAXIS values after the XAXIS Mandatory Value in a TrendSpec definition. Remember to include a comma at the end of the mandatory value before listing any of these optional values. Include a comma between each optional value’s definition.
Many of the optional XAXIS values are equivalent to the properties that you can specify using the Edit X Axis window on a Pre-Configured Trend. For further information on these properties, see Configure the X-Axis.
The optional values that you can specify within the XAXIS section are:
| XAXIS Optional Values | ||
|---|---|---|
| Identifier | Value Type | Comments | 
| StartTime (Only applicable if the <X-Axis Mode> is set to Absolute.) | DATE | Use to specify the earliest time period that is to be shown on the x-axis when the ad hoc Trend is first displayed. Specify the time and date in this format: StartTime = %23dd/MM/yyyy HH:mm:ss.SSS%23 
                                    Example:
                                 StartTime = %2321/11/2008 08:30:00.000%23 (Within a TrendSpec definition, a DATE value has to be enclosed within the code %23.) | 
| EndTime (Only applicable if the <X-Axis Mode> is set to Absolute.) | DATE | Use to specify the latest time period that is to be shown on the x-axis when the ad hoc Trend is first displayed. Specify the time and date in this format: StartTime = %23dd/MM/yyyy HH:mm:ss.SSS%23 
                                    Example:
                                 EndTime = %2322/11/2008 08:30:00.000%23 (Within a TrendSpec definition, a DATE value has to be enclosed within the code %23.) | 
| Offset (Only applicable if the <X-Axis Mode> is set to RelativeNow or RelativeLatest.) | String | Use to specify the earliest time that is displayed on the x-axis, in relation to the current time. You need to Specify a Relative Time in the OPC Relative Time Format. 
                                    Example:
                                 Offset = 'Hour - 3 Hours' (for the x-axis to display an interval that starts 3 hours before the start of the current hour) | 
| Interval (Only applicable if the <X-Axis Mode> is set to RelativeNow or RelativeLatest.) | String | Use to specify the amount of time that is displayed on the x-axis at one time. You need to Specify a Time Period in the OPC Time Format. 
                                    Example:
                                 Interval = '1 Hour' or Interval = ‘1H’ Alsosee Use TrendSpec to Define a Multiple Trace Ad Hoc Trend. | 
| Format | Identifier value | Use to specify the time format used for the x-axis. Specify one of these values: TwelveHour, or TwentyFourHour. 
                                    Example:
                                 Format = TwentyFourHour (If TwelveHour is specified, the time on the x-axis is appended with AM or PM, as applicable.) | 
| MinorTicks | Integer | Use to specify the number of minor tick indicators that are to appear between the major indicators on the x-axis. Enter a suitable value in the range 1 to 10 inclusive. 
                                    Example:
                                 MinorTicks = 3 | 
| Position | Identifier value | Use to specify the position of the x-axis on the ad hoc Trend. Specify one of these values: Top, or Bottom. 
                                    Example:
                                 Position = Bottom Alsosee Enable Users to Specify Which Traces to Include on an Ad Hoc Trend. | 
| Continuous | Boolean | Use to continuously scroll the x-axis when the time almost reaches the end of the time interval currently shown on the x-axis. In this mode, you can automatically follow the trend’s trace after it reaches the end of the current x-axis time interval. For more information, see Configure the X-Axis 
                                    Example:
                                 Continuous = True | 
| Jump | Boolean | Use if you want the x-axis to show (jump to) the time interval after the time interval currently shown on the x-axis. It will do this when the time reaches the end of the current x-axis time interval. For more information, see Configure the X-Axis 
                                    Example:
                                 Jump = True | 
| ShowGrid | Boolean | Use to specify whether vertical grid lines are shown for the major ticks on the x-axis. 
                                    Example:
                                 ShowGrid = False (Use the YAXIS ShowGrid identifier to specify whether horizontal grid lines are displayed (see YAXIS Optional Values).) | 
| ShowNow | Boolean | Use to specify whether a vertical line that indicates the values for the current time (‘now’) is shown on the Trend. 
                                   Example:
                                 ShowNow = False | 
| Colour | RGB | Use to specify the RGB color of the x-axis. 
                                    Example:
                                 Colour = RGB(0,0,0) |