Edit Tab

The Edit tab contains the following command groups:

The Save, Clipboard and Undo /Redo groups include commands that mainly apply to users with higher security permissions. The exception to this is the 'Save in Document Store' command, which you can use to Add a Copy of a Document to your Operator Document Store.

Copy and Paste limitations apply when you are using a Virtual ViewX client (see Use Copy and Paste in Virtual ViewX).

The Design group includes the Design Mode command, used by high-level users to switch between Run Mode and Design Mode while configuring database items.


Disclaimer

Geo SCADA Expert 2021