Suppression Status

Associated with: Any item for which an alarm can be raised, and on which Alarm Suppression is configured

This status attribute indicates whether Alarm Suppression is currently in force on the database item.

The possible states are:

Use this status attribute in conjunction with the Suppressing Parent status attribute (to ascertain the name of the database item that triggered the alarm suppression).

Further Information

Alarm Suppression: see Configure any Alarm Suppression Requirements in the Geo SCADA Expert Guide to Core Configuration.


Disclaimer

Geo SCADA Expert 2021