Configuring a WITS Binary Point

The Geo SCADA Expert WITS driver supports Binary Input, double-bit Binary Input, and Binary Output points. These binary points have a combination of configuration settings that are:

Pulse Actions are a specialization of binary outputs. For more information, Configuring DNP3 Pulse Actions.

To configure a WITS binary point, you need to use the Binary Input Point Form or Binary Output Point Form as appropriate.

WITS Binary Point Form

The Form contains many fields, organized into tabs. Some of these tabs are common to many types of database item, but the Binary Point tab contains settings that are specific to WITS.

The Control tab is only available on the Binary Output Form.

For information on the settings on the various tabs, please refer to the following topics:


Disclaimer

Geo SCADA Expert 2021