Scanning (WITS Outstation)

Associated with: WITS Outstations.

 

The Scanning attribute is a Health Check Status item. The attribute indicates whether the Field Device is On Scan or Off Scan.

When a Field Device is On Scan, the points in the Field Device will log data and generate events. However, you can set each point to Off Scan independently. Therefore, a Field Device that is On Scan may not log data or generate events for all of its points.

When a Field Device is Off Scan:

For more information, (see Set a WITS Outstation to be On Scan or Off Scan).

 

You can define whether a WITS Outstation item is set to On Scan or Off Scan in its initial configuration. To do this, you use the Enabled check box in the Scanning section of the WITS tab in the WITS Outstation Form ((see Set a WITS Outstation to be On Scan or Off Scan)). You should then download the configuration to the Field Device ((see Download Configuration (WITS Outstation))).

You can set a Field Device to be On Scan or Off Scan by using the On Scan (WITS Outstation) and Off Scan (WITS Outstation) actions.

Further Information

Set a WITS Outstation to be On Scan or Off Scan.

Scanning (WITS Point)

Scanning (WITS Pulse Action)


Disclaimer

Geo SCADA Expert 2021