WITS Driver-Specific <Update Type> Status Values

<Update Type> Status attributes such as Current Status and Previous Update Status are common to points on many drivers. They indicate the status of the particular point value to which the attribute relates (as opposed to providing general information about the status of the point itself). For example, a point’s Previous Update Status attribute only indicates the status of that point’s Previous Update Value.

For points on the WITS driver, <Update Type> Status attributes might display a combination of common values, DNP3 specific values and the following WITS driver-specific values:

 

With each of the above Status values, the associated Quality attribute should provide more information about the reliability of the point’s data and/or the source of the point value.

For further information about <Update Type> Status attributes and other attributes that are common to many types of point, see Status Attributes Associated with Points and see DNP3-Specific Status Display Attributes.

With WITS points for which Geo SCADA Expert stores data historically, the above Status values also appear in Historic Lists see WITS-Specific Status Descriptions on Historic Lists).


Disclaimer

Geo SCADA Expert 2021